Configuring Measurement Sweep Mode
The selection controls the sweeping operation of the VSA:
- , which performs consecutive sweeps without stopping.
- , which pauses the measurement after each sweep.
Continuous sweep
By default, the VSA performs consecutive sweeps without stopping. To initiate sweeping, click Restart. To pause and resume a measurement at any time, click Pause/Single.
Single sweep
When is set to , the VSA will pause the measurement after completing a single sweep.
To perform another sweep, click .
When averaging is on, clicking performs a sweep and includes the results in the current average, regardless of the number of averages specified by the Count parameter (unless is enabled; see Pausing and Single-Stepping a Measurement for more details).
When you click , the VSA resets averages, performs a single sweep, and pauses the measurement.
The measurement control buttons in the toolbar or in the menu only apply to the selected measurement. To start or pause multiple measurements, use the buttons on the Measurements dialog.
See Also
Disconnecting from Measurement Hardware
Configuring Measurement Sweep Mode
Starting and Stopping a measurement
Configuring Multiple Measurements